MAX31856MUD+: FAQ
问答
讨论
文档
Members
Tags
Cancel
文档
+
AD
+
ADG
+
ADM
+
ADUM
+
DS
+
General
+
MAX1x
+
MAX2x
-
MAX3x
MAX3051: FAQ
+
MAX3051EKA+: FAQ
MAX3078EESA+: FAQ
+
MAX3078EESA+T: FAQ
+
MAX3082: FAQ
+
MAX3085CPA+: FAQ
+
MAX3098E: FAQ
+
MAX3100CEE+: FAQ
+
MAX3107: FAQ
+
MAX3107EAG+: FAQ
+
MAX3108: FAQ
+
MAX3160CAP+: FAQ
MAX3160EAP+: FAQ
+
MAX3160EAP+T: FAQ
+
MAX3160ECAP+T: FAQ
+
MAX3162CAI+: FAQ
+
MAX31725MTA+: FAQ
MAX31740: FAQ
+
MAX31740ATA+: FAQ
MAX31855: FAQ
+
MAX31855EASA+: FAQ
+
MAX31855KASA+: FAQ
+
MAX31855NASA+: FAQ
+
MAX31856: FAQ
-
MAX31856MUD+: FAQ
MAX31856 设置为电压模式,增益为32时,如果输入电压小于-8mV左右将无法正常工作,为什么?
MAX31856如果外部没有连接热电偶,芯片的冷端温度也无法转换,当接上热电偶后,冷端温度可以正常输出,即使再断开热电偶,冷端温度也能正常输出,这种现象正常吗?
MAX31856芯片前面加复用器实现多通道测温,长时间测温后断电再立刻上电重启,芯片会不工作,没有温度读数和DRDY引脚信号。必须断电超过30s再上电重启恢复正常工作,请问怎么解决。
为降低系统工作电流,在设计时将MAX31856设置为单次转换(ON Duty 1/60),但是在对多个器件进行测试静态电流时发现电流为10uA--500uA之间不等,数据手册说静态电流为5.25uA.这个和数据手册不符,请问是什么原因?
利用热端接地的K型热电偶进行温度采集,在设计电路中采用MAX31856时,应该如何处理?
在使用MAX31856时,初始化和测温都正常,但是无法检测温度传感器开路,如何解决?
在使用MAX31856时,在上电时偶尔会出现OV/UV Error,通过Auto Reset Error无法解决。是什么原因?
在使用Max31856测量温度时,如果MAX31856与热电偶sense端有一段距离且板温度与感测端温度不同,是否会对测量温度产生误差?
实验室测试max31856读取热电偶的温度正常,安装到整机后发现MAX31856读取的温度结果跳动很大,请问如何解决?
我们使用STM32F4的单片机通过SPI接口与MAX31865通讯,正常工作时没问题,当我测试PT100开路时,错误码返回0x80(超过上门限),但是当我把PT100接回去后错误码依然存在,还是0x80;测试短路时,错误码显示为0x84,也就是说当错误消除后,错误码仍然存在,需要手动清零错误吗?
用HIOKI SS7012模拟热电偶在-170C时的输出电压,然后用MAX31856 evkit测量,得到的热电偶温度为-121.3C,冷端温度为29.2C,-170C+29.2C=-140.8C,和MAX31856EVKIT测量到的误差达到了19.5C,为什么误差会这么大?
+
MAX31865AAP+: FAQ
+
MAX31865ATP+: FAQ
+
MAX31865EVKIT#: FAQ
+
MAX31913AUI+: FAQ
+
MAX3221EEAE: FAQ
+
MAX3222EEUP+_T1: FAQ
+
MAX3223EEUP+T: FAQ
+
MAX3232CAE_T1: FAQ
MAX3232E: FAQ
+
MAX3232ESE+T: FAQ
MAX3232ESE: FAQ
+
MAX3243CAI+T: FAQ
+
MAX3243E: FAQ
+
MAX3250CAI+: FAQ
+
MAX3280E: FAQ
+
MAX3284E: FAQ
+
MAX3362EKA+: FAQ
MAX3387ECUG+: FAQ
+
MAX3387ECUG+T: FAQ
+
MAX3420EECJ+: FAQ
+
MAX3421EEHJ+: FAQ
+
MAX3444EASA+: FAQ
+
MAX3471: FAQ
+
MAX3483AE: FAQ
+
MAX3485: FAQ
+
MAX3490CSA: FAQ
+
MAX3815ACCM+: FAQ
+
MAX4x
+
MAX5x
+
MAX7x
+
MAXM
MAX31856MUD+: FAQ
MAX31856MUD+: FAQ
Share
History
More
Cancel
Related
Recommended
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.