Post Go back to editing

Adum5000/6000使用问题

ADI的工程师,你们好!

我目前在开发一款产品,使用到贵公司的电源隔离芯片,ADUM5000/6000。电路图如下:

UISO3工作在master模式,UISO4/5工作在slave模式,目的是为了若电流不足,UISO4和5可以补充供电。

目前焊接了UISO3和UISO4,UISO5暂未焊接。焊接后测试发现这两颗芯片发热严重。请帮我检查一下电源隔离部分是否设计有问题?

我检查了datasheet,pin1和pin7内部连接,但是裸片时用万用表测试发现有约50K左右的电阻,pin10和pin16也是同样情况,请问是否正常?对了,目前使用ADUM5000这个芯片。

谢谢!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.