大家好,我想设计一个医用高速DAC激励信号源,直接通过电极作用于人体,然后用4片AD4003进行采集。整体电路需要满足IEC 60601医用仪器隔离标准。但是对于高速DAC的隔离和多片ADC的隔离,有几个疑问希望ADI的专家和版上的大牛们能帮助解决:
1、管脚数目较多时的隔离需求。高速DAC一般具有较多的管脚数目,例如拿AD9744而言,需要14路信号,1路时钟,3路控制(MODE,SLEEP,CMODE)。一般而言,一个ADuM隔离芯片最多支持4到6路信号,那么针对高速DAC应用,至少需要3到4片ADuM隔离芯片;而针对更高速率的DAC,例如AD9125而言,光DAC数据就需要16对共32个管脚。那么,针对管脚数目较多、需求ADuM芯片较多时,应该怎么设计隔离呢?
2、ISO隔离端功耗较大。对于AD9744,典型功耗是135mW(3.3V),而我又想用ADuM实现简单的隔离和供电,因此芯片集中在ADuM5000和ADuM6000系列,输出电流分别在70mA到50mA之间,整个DAC信号链包含1个AD9744,1个AD5683R,4个运放,一个多路选择,这样来看,供电是不是跟不上呢?ADI有没有针对较大隔离负载的解决方案呢?
3、在隔离端有多个电压轨。在隔离端,需要正负5V、正负12V,3.3V和1.8VA,那么是不是需要在隔离端进行DC转换呢?这样会不会进一步降低效率,导致隔离部分供电不足呢?请问针对这种情况,有没有较好的隔离方案呢?
谢谢各位专家啦!期待回复~~