Post Go back to editing

MAX96701 MAX96712/96722

Thread Summary

The user inquired about the communication compatibility between MAX96701 and MAX96712 or 96722. The final answer confirmed that communication is possible. No additional technical parameters or workarounds were specified.
AI Generated Content
Category: Hardware
Product Number: MAX96701

Hello,

Can MAX96701 communicate with MAX96712 or 96722

thank you

Thread Notes