Post Go back to editing

MAX22216

Thread Summary

The user is experiencing a HHF fault when using the Max22216 to control an electromagnetic valve in CDR mode with VM at 24V and a 240Ω resistor. The final answer suggests checking if the current ever reaches 90mA and adjusting both Kp and Ki parameters, as the issue may be due to inappropriate PI settings.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX22216

我在使用Max22216控制电磁阀时,VM为24V,电磁阀电阻为240欧,我使用CDR模式进行闭环控制,我设置DC_L2H为90mA,DC_H为60mA,最终电流稳定在60mA,但会产生一个故障告警HHF,调大L2H_TIME或者改大kp,仍然报这个错误,调小DC_L2H的值,问题依旧存在。

  • 我重新研究了一下您的问题。 在CDR模式下这个报错,就是没有达到您设置的90mA。您可以实际检测一下电流是否曾经到达过, 对于电流的调整可能需要您同时调整Kp和Ki, 对于CDR模式,DCL2H和DCH这两个都是CDR,所以我认为可能就是PI的参数不是很合适导致的。 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.