Post Go back to editing

MAX31855 Thermocouple-based anti-interference methods and measures

Thread Summary

The user experiences temperature measurement errors with the MAX31855 near a switching power supply transformer. The solution involves installing 10nF ceramic capacitors between T+ and T-, and 10nF decoupling capacitors between T+ to GND and T- to GND. Adding small ferrite beads or series resistors (< 1000Ω) can also help filter high-frequency noise (> 100MHz). Large copper areas on the PCB can provide additional noise reduction.
AI Generated Content

I'm using the MAX31855 to measure temperature, and when close to the transformer of a switching power supply, a serious temperature error occurs, and I'd like to know how to avoid this interference caused.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.