I'm using the MAX31855 to measure temperature, and when close to the transformer of a switching power supply, a serious temperature error occurs, and I'd like to know how to avoid this interference caused.
I'm using the MAX31855 to measure temperature, and when close to the transformer of a switching power supply, a serious temperature error occurs, and I'd like to know how to avoid this interference caused.
Moved from Power Management to 接口和隔离专区 on Tuesday, November 21, 2023 12:24:43 AM by frank_huang
应在靠近MAX31855封装的位置,在T+和T-引脚之间安装10nF(最大值)陶瓷电容;在T+至GND以及T-至GND之间安装10nF去耦电容(最大值)。 与MAX31855评估板类似,可增加小磁珠或串联电阻(< 1000Ω),有助于滤波。然而,对于高频噪声(> 100MHz),MAX31855的ADC将产生较大失调的读数。
你好,我用的31855设计的K型热电偶检测电路,测试时发现这么个问题:
有一路热电偶检测温度不稳定,来回跳动。与其他通道交换传感器,发现是传感器问题。将问题传感器接到欧姆龙温控器上,却显示正常,问题传感器接回31855,仍旧跳动。后发现热电偶补偿导线中间折弯了,将折弯缕直后显示正常。
能帮分析一下会使什么问题吗,为什么在欧姆龙温控器却显示正常。
我的电路如下:

我看您也有滤波. 滤波器件是否是靠近31855? 另外能否修改filter的值, 比如将电容改小?
我看您也有滤波. 滤波器件是否是靠近31855? 另外能否修改filter的值, 比如将电容改小?
滤波器靠近31855,见下面截图。等下一版我将电容改小试试。
这几天又验证了一下,就是热电偶弯折的角度大一些,就会出现温度值乱跳的情况,譬如室温26度,会在17度到26度之间跳动。把热电偶捋直就正常。


你好,我在基板上用AD8495和MAX31855,做对比,来确定最终用哪个芯片。现在有个问题,一共4路MAX31855,有2路在变频器启动后有明显的温度降低,比正常的2路低4-5度,关掉变频器就恢复正常。
另有2路AD8495,很正常。
麻烦帮分析一下,这种情况怎么处理。
附图纸:

补充一下,4路MAX31855,2路正常不受变频干扰的滤波电容,即T+与GND、T-与GND,均为0.1uf。另两路按照咱网站上厂家建议,改成了0.01uf,就是改成0.01uf的2路受变频干扰。