Post Go back to editing

MAX31855 Thermocouple-based anti-interference methods and measures

Thread Summary

The user experiences temperature measurement errors with the MAX31855 near a switching power supply transformer. The solution involves installing 10nF ceramic capacitors between T+ and T-, and 10nF decoupling capacitors between T+ to GND and T- to GND. Adding small ferrite beads or series resistors (< 1000Ω) can also help filter high-frequency noise (> 100MHz). Large copper areas on the PCB can provide additional noise reduction.
AI Generated Content

I'm using the MAX31855 to measure temperature, and when close to the transformer of a switching power supply, a serious temperature error occurs, and I'd like to know how to avoid this interference caused.

Thread Notes

Parents
  • 应在靠近MAX31855封装的位置,在T+和T-引脚之间安装10nF(最大值)陶瓷电容;在T+至GND以及T-至GND之间安装10nF去耦电容(最大值)。 与MAX31855评估板类似,可增加小磁珠或串联电阻(< 1000Ω),有助于滤波。然而,对于高频噪声(> 100MHz),MAX31855的ADC将产生较大失调的读数。

  • on Sep 24, 2025 11:27 AM in reply to koko1230 Contains AI Generated Content
    0

    你好,我用的31855设计的K型热电偶检测电路,测试时发现这么个问题:

    有一路热电偶检测温度不稳定,来回跳动。与其他通道交换传感器,发现是传感器问题。将问题传感器接到欧姆龙温控器上,却显示正常,问题传感器接回31855,仍旧跳动。后发现热电偶补偿导线中间折弯了,将折弯缕直后显示正常。

    能帮分析一下会使什么问题吗,为什么在欧姆龙温控器却显示正常。

    我的电路如下:

Reply
  • on Sep 24, 2025 11:27 AM in reply to koko1230 Contains AI Generated Content
    0

    你好,我用的31855设计的K型热电偶检测电路,测试时发现这么个问题:

    有一路热电偶检测温度不稳定,来回跳动。与其他通道交换传感器,发现是传感器问题。将问题传感器接到欧姆龙温控器上,却显示正常,问题传感器接回31855,仍旧跳动。后发现热电偶补偿导线中间折弯了,将折弯缕直后显示正常。

    能帮分析一下会使什么问题吗,为什么在欧姆龙温控器却显示正常。

    我的电路如下:

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.