Post Go back to editing

ADM3055E 信号台阶问题

Thread Summary

The user observed a 140ns step in the CAN signal's start bit, which is a known behavior of the ADM3055 transceiver. This occurs after the transceiver has been in the recessive state for more than 25ms, due to an internal protective circuit being incorrectly triggered. The issue does not affect the functionality of the CAN communication as the VOD remains sufficient for dominant state recognition. This characteristic is also present in other transceivers using the same die, such as ADM3050E, ADM3056, ADM3057, and ADM3058.
AI Generated Content

 按照手册推荐电路搭建的CAN控制器电路,在系统中测试信号发现信号侦的起始位上升沿始终存在一个约140ns的台阶,而后面的数据位都没有这个台阶。是因为芯片DCDC电源驱动能力问题吗?

Parents
  • Hello Laocali,

       This step is caused by a known 'feature' of the ADM3055 which is unrelated to the on-chip dc-dc power supply.  The first bit in the arbitration phase will have this notch or step when the transceiver has been in the recessive state for longer than approx. 25ms.  The level of the notch can vary based on the amount of time in the recessive state, but the time of the notch will remain the same. 

       The cause of the behavior is well understood and is consistently repeatable.   While this behavior isn’t desired or ideal, it also has not caused any actual functional issues or problems in practice since the reduced VOD remains large enough for the other nodes to still recognize the dominant state.

    Eric

  • Hi Eric ,Is this  'feature'  unique to ADM3055E? Or do all controllers have it? What is the reason for its occurrence?

  • This is unique to the ADM3055's transceiver die (and the other parts which use this same die - ADM3050E, ADM3056, ADM3057 and ADM3058).   

    When the transceiver has been in the recessive state for longer than approximately 25ms, it is possible for an internal protective circuit to be incorrectly triggered for a brief time causing a contention between the output driver and the protective circuit which results in the notch observed in the output CANH waveform.

Reply
  • This is unique to the ADM3055's transceiver die (and the other parts which use this same die - ADM3050E, ADM3056, ADM3057 and ADM3058).   

    When the transceiver has been in the recessive state for longer than approximately 25ms, it is possible for an internal protective circuit to be incorrectly triggered for a brief time causing a contention between the output driver and the protective circuit which results in the notch observed in the output CANH waveform.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.