Post Go back to editing

ADM2682E不能发送数据

我正在使用ADM2682E作为RS422进行通信,对方是5V的485模块,我把ADM2682E的AB和对方485的AB对接,可以正常接收到对方发送的数据,但是我把YZ和对方485的AB对接,对方收不到我发送的数据,请问这是什么原因造成的?我把ADM2682E的AB和YZ对接,也无法完成自发自收。

我量了YZ上的波形,数据波形看起来是对的,不过最高电压只有3.3v,这种情况是不是和5V的485就是无法通信?

图中Y和Z的波形是相对于GND2的。

备注:我的应用电路中是把两个ADM2682E的AB、YZ并在一起跟对方的485通信的,DE和RE和拉死了,两个芯片均一直处于可发送和接收的状态(实际测试时只有一个芯片发送数据),会跟这个原因有关吗?