我是一名自由硬件开发者,在一个小型板卡中拟使用Maxim-DS26503/DS26504作为2.048Mbps HDB3 transceiver和CDR组件。
我在Maxim提供的AN590(已添加附件) FAQ文档中注意到
Q16. Can I modify the codes of Maxim telecommunication drivers? A16. No. Maxim has the license of the driver that allows us to provide the driver code to the customers, but it does not change the ownership of the driver nor put it under the GNU licensing schemes. The customer can extend the driver through the macros or other recommended function commands.
请问如何申请C或verilog形式的DS26503/DS26504驱动代码或驱动程序?