MPU采用四线制spi与DC1941评估板相连,采用外部供电5V(从MPU上取电),PHA与POL都设为1,速度为快速,JP9与JP10均设置到VTH1,JP3设置为EN,通过示波器可以观察到长+1、长-1与短-1三种类型的脉冲类型,但是就是观察不到短+1的波形,通过逻辑分析仪可以明确看到有MOSI=1的输出,但是经过LTC6820后就看不到这样的短+1波形
就是从示波器上看不到这样的短+1波形
问题已解决:将DC1941评估板的Vdd要外接3V,而不是5V。外接3V后可以正常工作,就可以看到短+1的波形