Hi,
Does the 'ON' on LTM2810-S turn off the power to the isolated side? when the 'ON' is logic HIGH, what is the state of input and output pins on the isolated side?
ST1, ST2 (A6, C6): Bridge Driver Outputs, Referenced
to PVCC and GND. Each output runs at 50% duty cycle,
ST1 is 180 degrees out of phase with ST2. Operating
frequency is 2MHz. Bridge driver is enabled when PVCC
is between 3V to 5.5V and ON is high.
Please let me know, thanks!
Regards, =Su=