MAX3160电路,如果只使用1TX/1RX RS232通信,是否可以使用TX1和RX2,或必须使用TX1/RX1或TX2/RX2?
文档
Forums
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
8 months ago
文档
MAX3x
MAX3160ECAP+T: FAQ
MAX3160电路,如果只使用1TX/1RX RS232通信,是否可以使用TX1和RX2,或必须使用TX1/RX1或TX2/RX2?
MAX3160
可通过引脚设置为
2TX/2RX RS-232
或半双工
/
全双工
RS-485
收发器。一旦使能
RS-232
功能,用户可以使用
RX1/TX1, RX2/TX2, RX1/TX2
或
RX2/TX1
。
MAX3160ECAP+T
000094319
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.