Article MAX22190是否可以设计为同时支持Type1,2和Type3的信号输入?

 对于Digital IO,通常都时24V的信号,为了兼容Type 1,2 ,3 的规范,虽然对于输入的高电平限都是一样的,但是对于Type1,3和Type2 的吸入电流定义是不一样的,可以看到对于Type2是外接电阻是1K(2个通道并联使用),Type1,3 是1.5K,因此,可以设计为8通道 Type1和Type3, 或者4通道Type2, 但不能同时支持Type1,2,3. 这和吸入电流的定义有关。

 
 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.