MAXM22510GLH+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAXM
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAXM22510 如果输出发生短路,器件内部是如何处理短路故障的?
MAX22510内部对于短路保护采用两层保护,当短路发生时,内部的限流电路会立即动作,把短路电流限制到设定的限值,在这种情况下,由于短路电流很大,如果短路状态一直持续,会使器件发热,内部的热保护电路会在器件管芯温度超过160C触发热关断,热关断会将输出设置为高阻状态并且将VDDB下电到0V。
MAXM22510/MAXM22511内部电源的工作频率是多少?它是如何改善EMI的?
MAXM22510/MAXM22511内部变压器驱动工作频率为450kHz左右,用于产生隔离电源的变压器基于铁氧体磁芯,有助于改善EMI。其内部电源在效率、EMI性能上均优于目前市场同类产品。
MAXM22510EVKIT利用4层板设计改善EMI,如果采用2层板需要注意哪些问题?
MAXM22510评估板提供了两个版本:带缝补电容和不带缝补电容,均采用4层板PCB。根据我们的EMI测试结果,不带缝补电容的电路板仍然有很好的EMI性能,并且可以通过CISPR ClassB,区别在于缝补电容有助于减小800-1000MHz频带的高频噪声。如果可以接受MAXM22510的辐射比classB的要求低8dB,则可以使用两层电路板设计。设计两层电路板时,为确保EMI性能,请注意围绕GNDA和GNDB增加边沿保护过孔…
MAXM22510的RX/TX仅支持3.3V电平,如果和5V的控制器之间通讯,是否需要电平转换器?
对于MAXM22510 TXD,该引脚为输入引脚,可以支持5V的电压,但是对于RXD,该引脚为输出,输出的最大电压由VDDA决定(VDDA-0.4V),这个输出信号到5V的系统后,如果系统能够将(VDDA-0.4V)识别为高电平,则无需电平转换,否则需要电平转换器。
MAXM22510能够提供的隔离电源输出功率是多大?
MAXM22510的隔离电源侧集成了LDO(VDDB),LDO最大输出功率为1W(典型值:3.3V@300mA)。该隔离电源输出用于RS485总线侧供电,不推荐为其他元器件供电。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.