MAX77860EWG+T: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX7x
Created
over 5 years ago
Was this helpful?
Yes
No
More
Cancel
MAX77860在电池充电的同时,是否也可以给BYP管脚供电?
MAX77860支持这种模式,寄存器0xB7选择MODE = 0x0D,BATT充电的同时,提供VBYP = VCHGIN - IQCHGIN x RIN2BYP。 具体请查看规格书Page43的Figure9
MAX77860是否可以通过CC pin检测Alt mode下的Display Port接口?
MAX77860的CC检测不支持HDMI、DisplayPort这些Alt mode功能,可以支持CC charger和Audio accessory的检测
MAX77860的CC pin是否可以不接, 仅通过D+/D-来控制充电行为?
可以的。 MAX77860可以支持USB BC(Battery Charger) 1.2协议的检测。
MAX77860芯片的0xB7寄存器配置MODE=0x0A以后,为什么无法实现OTG功能?
启动MAX77860的OTG功能,需要将0xB7的Bit7 DIS_USBC_CTRL写为0(Enable)
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.