MAX7360ETL+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX7x
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX7360对于多按键同时按下是否有限制?
MAX7360对于同时按下几个按键没有限制,除非按键在相邻矩形上(所谓的ghost-key,如附件所示)或者FIFO存满了。关于多按键同时按下的操作,中断响应、按键按下的时间之间需要配合好。第一个按键按下时,即触发中断。如果中断响应响应第一个按键按下操作,第二个按键按下尚未完成(考虑去抖延时),则有可能读不到第二个按键的状态。需要客户在中断响应、去抖时间上做些调试。
在测试时发现MAX7360消耗电流430uA,此时器件没有连接任何LED,而数据手册给出的参考值是34uA,造成这一差别的原因是什么?
数据手册给出的34uA是在 COL2--COL7 配置为按键开关时测量的,MAX7360上电的默认状态是COL2--COL7设置为GPO端口,需要设置0x02寄存器为00,将COL2--COL7 配置为按键开关。然后再进行测试。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.