MAX4950ACTX+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX4x
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX4950A有两个通道A和B,是否只有通道A和通道B同时输入有效信号的时候,MAX4950A才处于工作模式?
不是,启动输入检测后,一旦检测到一个通道的接收信号,将最多尝试在另一通道检测三次。然后使能通道输出以及信号空闲检测。
关于MAX4950A的接收检测,是否只要将MAX4950A的EN信号置为高电平,那么MAX4950A就会进入接收检测模式,而不用考虑RX_DET处于什么输入信号?如果是这样的话,那么RX_DET输入有什么作用呢?
利用RX_DET可以节省功耗并降低噪声,如果器件上电后,在需要检测输入之前不必拉高EN。需要检测输入时,拉高EN,然后由RX_DET的上升沿或下降沿启动输入检测,输入信号检测期间,器件处于待机状态(即使EN为高电平)并禁止输出信号。
请问MAX4950A的差分输入引脚是否可以极性反接?
如果反接,在接收器端也要反相。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.