MAX491: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX4x
Interface Transceivers & Isolators
MAX491
Created
over 8 years ago
Updated
1 month ago
Was this helpful?
Yes
No
More
Cancel
MAX491未上电时,A/B输入和Y/Z输出是什么情况?仍然保持为高阻吗?或者,是否通过ESD二极管等将线路下拉至0V?
一般情况下,RS-485收发器未加电时,接收器输入呈现特定的输入电阻(对于MAX491而言,如数据资料所述,最小为12kΩ),发送器输出为高阻。这样可防止收发器在未加电时将整个RS-485总线拉低。
MAX491采用5V供电,处理器采用3.3V供电,请问MAX491是否可以和3.3V逻辑兼容,是否需要电平转换器?
对于MAX491,可以接收3.3V的逻辑电平,但是MAX491的输出到处理器为5V逻辑,此时要确保处理器在3.3V供电时可以承受5V的逻辑电平,否则就需要电平转换。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.