MAX489CSD+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX4x
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX489与MAX3083的失效保护电路有何区别?
MAX489与MAX3083采用不同的失效保护电路: 对于MAX489,其内部为弱上拉、下拉架构。只有当总线开路时,才能保证接收器输出为高电平。 如果在A、B间连接120欧姆电阻,则在总线开路时将A、B间电压拉至0V,从而导致接收器输出不确定。这种情况下,应在外部对A线、B线分别加上拉、下拉电阻。 MAX3083的失效保护电路则将接收器高电平输出对应的总线输入电压门限移至-50mV…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.