MAX3471: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
Interface Transceivers & Isolators
MAX3471
Created
over 8 years ago
Updated
17 days ago
Was this helpful?
Yes
No
More
Cancel
MAX3471 RS485输出阻抗是多少?
按照RS485标准要求,RS485发送器应该驱动总线上32个节点(输入阻抗12k)以及2个120ohm匹配电阻。 关于MAX3471输出阻抗,由数据手册可知:Tx输出开路电压为VCC。 驱动器输出短路电流为: 由此可得: RO = 3.6V / 60mA = 60ohm (VCC = 3.6V) RO = 5.5 V/ 130mA = 42ohm (VCC = 5.5V) 答案是:40 - 60ohm…
MAX3471在电源未上电时,如果A和B之间施加有信号,是否会损坏器件?如果器件不损坏,RO输出是什么信号?
在MAX485器件上进行测试,测试条件如下:电源输入悬空,电源和GND之间连接0.1uF电容,B接GND。对A施加不同电压时监测电源电压以及RO输出电压的结果: A=2.4V VCC=1.2V OUT=0.22V A=5V VCC=1.7V OUT=1.73V A=8V VCC=2V OUT=2V A=10V VCC=2.2V OUT=2.2V 从测试结果来看,在器件未上电时,当A B之间施加电压…
MAX3471端接电阻如何选择?
RS485端接电阻与使用的传输线有关,等于传输线的特征阻抗。通常为110 - 130欧姆。是否对RS-485总线进行终端匹配取决于数据传输速率、电缆长度及信号转换速率。UART是在每个数据位的中点采样数据的,只要反射信号在开始采样时衰减到足够低就可以不考虑匹配。有一条经验性的准则可以用来判断在什么样的数据速率和电缆长度时需要进行匹配:当信号的转换时间(上升或下降时间)超过电信号沿总线单向传输所需时间的3倍以上时就可以不加匹配…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.