MAX3420E中的SPI接口为3、4或5线是什么意思?
文档
Forums
Members
Tags
Cancel
Was this helpful?
Was this helpful?
Yes
No
In this Article
Created
over 8 years ago
Updated
9 months ago
文档
MAX3x
MAX3420EECJ+: FAQ
MAX3420E中的SPI接口为3、4或5线是什么意思?
最简单的SPI接口包括三条线:SS#(从机选择)、SCLK(串行时钟)和MISO(双向MISO/MOSI数据配置)。由于该接口不使用INT引脚,控制微处理器需要查询两个中断请求寄存器来确定MAX3420E什么时候需要服务。通过设置控制位(FDUPSPI,全双工SPI),使MOSI和MISO数据出现在不同引脚上,可实现4线接口。最后,一个INT(中断输出)引脚可连接处理器的中断系统。
MAX3420E
000102159
接口和隔离专区
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.