MAX3387ECUG+T: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
MAX3387ECUG+T: FAQ
MAX3387ECUG+T: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX3387E Tx输出对地短路,是否会损坏器件?
MAX3387E T3OUT输出对地短路时,器件不一定损坏,但由于电荷泵输出电压V+、V-不能提供足够的驱动,将影响T1OUT、T2OUT的输出电平。
使用MAX3387EEUG+,发现在环境温度为0摄氏度及以下时输出开始异常,如何解决?
MAX3387EEUG的工作温度范围是:-40°C to +85°C。低温下,如果不低于-40°C,导致RS232通信异常的原因很可能是外部电容造成的。MAX3387E内部电荷泵工作时所要求的最小外部电容值如下表所示。如果电容的温度特性较差,低温下容值低于下表所列参数,则会导致发送器输出错误。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.