MAX31855NASA+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX31855使用哪种SPI模式?
MAX31855提供一个只读的模式1 SPI接口。
MAX31855和MAX6675这两款芯片有何区别!
MAX6675 MAX31855 供电: +3.3V--+5V +3.3V ADC: 12位 14位 测量范围: 0C-1024 C -270C--+ 1372 (K型) 支持类型 K 各种类型,取决于器件的尾缀 硬件连接 T- 接GND T-悬空 故障检测 开路 开路/短路 输出数据 热电偶温度 热电偶温度,冷端温度,故障状态 由于热电偶本身是非线性输出,但是这两款产品均未提供热电偶输出的线性补偿…
MAX31855对热电偶测量结果进行线性化吗?
MAX31855内部没有线性化处理功能。尽管MAX31855执行自动冷端补偿,但不执行线性化计算。对热电偶结果进行线性化需要外部处理器执行NIST计算: http://srdata.nist.gov/its90/main/ 作为替代方案,MAX31856内置对所有支持热电偶类型的线性化功能。
利用多片MAX31855实现多通道热电偶测温,多片MAX31855的T-可以连在一起吗?
不可以,必须要保证每个MAX31855独立测量每个通道的热电偶,各个热电偶之间保持独立,不能够将T-连接在一起。
测试MAX31855N时发现用调试器JTAG供电,测量温度误差较小;当采用外部5V供电时,测量到的温度偏差达到9度,分析发现冷端温度升高,造成这种现象的原因是什么?
MAX31855N的供电电源为3.3V,不能采用5V供电电源,如果MAX31855N采用3.3V供电,而处理器采用5V供电时,输出的逻辑高电平会比MAX31855N的供电电源电压还高,这样内部的保护二极管会导通,造成器件内部发热导致冷端温度升高,因此,请确认和MAX31855N通讯的器件也要采用3.3V供电或者采用电平转换器为MAX31855N提供符合要求的电平。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.