MAX3160EAP+T: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX3160E中RS232和RS485全双工和半双工模式控制是否可以实时切换而不需要重新上电下电?
全双工和半双工模式的切换是靠引脚的电平来决定的,可以实时切换,通常情况下,在一个上电周期内的通讯模式是不会变化的,因此,在开始通讯之前,通讯模式是必须预先设置好的而且在整个通讯期间是不会发生变化的。对于RS232而言,通常设置为全双工模式,但是可以采用半双工的模式进行通讯。
MAX3160E数据手册中特别说明该器件不支持RS232和RS485双模,如何理解该器件作为多协议收发器,却又不支持双模?
MAX3160E数据手册选型表如下,其中MAX3160E和MAX3161E不支持双模,即这两款器件只能配置成RS232模式,或者RS485模式。不能同时提供RS232和RS485总线支持。如需同时支持RS232、RS485通信,建议选择MAX3162E。
MAX3160在设置为485模式的半双工情况下(232模式收发没问题),远端外设发送的数据,我这边可以收到,但是我这边发送出的数据自己也可以收到。
MAX3160没有RE控制引脚,因此在RS485模式下,如果利用MAX3160发送数据时,MAX3160本身也会接收到数据,如果想要在发送数据是不接收到数据需要在外部增加一个逻辑器件来控制接收,例如或门,或门一个输入接MAX3160的输出,另外一个接控制信号。
MAX3160在设置为485模式的半双工情况下(全双工还没有进行测试,232模式收发没问题),远端外设发送的数据,我这边可以收到,但是我这边发送出的数据自己也可以收到。
MAX3160没有RE控制引脚,因此在RS485模式下,如果利用MAX3160发送数据时,MAX3160本身也会接收到数据,如果想要在发送数据是不接收到数据需要在外部增加一个逻辑器件来控制接收,例如或门,或门一个输入接MAX3160的输出,另外一个接控制信号。 当MAX3160处于RS485接收模式时,需要将DE485置低,此时MAX3160处于接收模式,否则会有数据冲突。
关于MAX3160E芯片作为RS485/RS422,RS232使用情况下,外接保护电路如何选择?
MAX3160E的RS232的输入和RS485的AB线可以承受最大+/-25V的电压,RS232的输出和RS485的YZ可以承受最大+/-13.2V的电压,为兼容RS232和RS485, TVS管要选择双极性,耐压10V即可,这样可以兼容大部分RS232接口。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.