MAX3107: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX3x
Interface Transceivers & Isolators
MAX3107
Created
over 8 years ago
Updated
18 days ago
Was this helpful?
Yes
No
More
Cancel
MAX3107 数据手册说SPI模式支持mode0,请问是否也支持mode3?
MAX3107 SPI通讯时仅支持mode0,不能够支持mode 3,因此,在和MAX3107进行SPI通讯时必须采用mode 0.
MAX3107使用外部晶振,是否需要加电容?
不需要,MAX3107内部谐振槽路集成了20pF的片上电容。
MAX3107在sleep模式下clkout是否输出时钟?
MAX3109在forced sleep模式下clkout不可以输出,在Autosleep模式下可以输出。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.