• Created
Was this helpful?
  • MAX3100 REV2.0图6修订

    MAX3100数据手册Rev 2; 1/09的图6存在错误,特说明如下: 1. /TM位为低时,同样可以设置T位为高;但发送缓存器空不会触发中断,除非、TM位置高。 2. /RM位置0时,R位可以置1;但收到数据时不会触发中断,除非/RM为“高”。
  • 从MAX3100读取数据时,为什么会有垃圾数据?

    MAX3100会在FIFO中储存之前使用的字节(所选字节通常是发送到器件的第一个字节;然而当FIFO溢出时,很难预测保存的是哪个字节),即使已经读取FIFO中的全部有效数据。如果您继续从FIFO读取数据,将仍然能够从中读取一个字节(不是0xFF或0x00)。 在从FIFO读取数据时(使用写数据寄存器或读数据寄存器),应使用数据中断(写配置中,/RM\ = 1)检测FIFO中何时不再有数据。该中断将区分FIFO中的实际字节何时为空…
  • 可否提供UART与半双工RS485的连接图?

    下图为UART与半双工RS485的连接图,供参考:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.