文档
MAX22025AWA+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX2x
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX22025的上、下拉电阻如何选取?
电阻选择的依据是确保总线空闲时,VA – VB > 200mV。 如果是按照n个节点的总线架构连接网络,每个节点的上拉/下拉电阻为R,则计算公式为: VPU x (RT/2)/[RT/2 + 2 x R/n] > 200mV 节点数多时,多个上拉,下拉电阻并联。为减轻总线负载,应尽可能选择大阻值R。
使用MAX22025 RS485收发器,允许总线上挂接多少个节点?
可以挂接32个节点。 如果只在总线两端加端接电阻和上、下拉电阻,中间其它节点只是加弱上、下拉或者不加上、下拉电阻,可以连接最多64节点。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.