MAX2021ETX+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX2x
Created
over 8 years ago
Was this helpful?
Yes
No
More
Cancel
MAX2021芯片用作解调器时,输出的基带应该如何处理?
MAX2021的I/Q输出为电压输出,数据手册提供了一个接口电路,请参考附件。 Ca = 1.5pF; Cb = 4.7pF La = 11nH Ra = 50Ω Rb = 50Ω to 200Ω Ce为隔直流电容 其余Cc, Cd,Lb, Lc可以不接。 ADC之前应加缓冲器。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.