MAX14917AFM+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
Created
over 5 years ago
Was this helpful?
Yes
No
More
Cancel
按照数据手册的推荐电路设计MAX14917,当输出使能后,可以测量到24V输出,但是输出关断后,在OUT上还可以测量到17V的电压,为什么?
根据MAX14917的推荐电路设计,在OUT输出引脚连接有10nF电容,当输出高后,24V电压对该电容充电,如果OUT没有连接负载,当断开后,由于是高边开关,内部为高阻抗,所以外部10nF电容存储的电能使得可以在OUT引脚测量到17V,如果此时在OUT上带有负载,则当开关打开后,负载对电容放电,应该就能得到一个很低的电压。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.