• Created
Was this helpful?
  • MAX14912电路中,通断24V 电源时输出出现一个2.32V、400us 脉冲,导致负载灯微闪,什么原因造成的?

    MAX14912内部电荷泵在上电时存在一个小电流 (<100uA),电荷泵不受关断控制,故在上电时出现一个瞬间的扰动脉冲: VDD电源上电速度对该脉冲的宽度有影响: VDD爬升速度较慢时,如果 EN = low,在推挽或高边模式下的输出端可以看到大约300us的扰动脉冲(带/不带负载);如果 EN = high,不带负载时,可以看到大约6ms的输出脉冲,带1kohm输出负载时,输出脉冲大约300us…
  • MAX14912的最高开关频率是多少?

    我们的数字输出器件(DO)在PP模式下开关频率最高,可以支持到200kHz, 此时输出需要通过并口控制。使用SPI接口无法支持高达200kHz的开关频率。 另外,推挽输出常常用于驱动容性负载,此时,最高开关频率不仅取决于MAX14912的驱动电路,还取决负载电容的大小。按照MAX14912数据手册,驱动100pF容性负载时,下降和上升时间分别为0.3us,考虑到波形的稳定性, 可以计算出MAX14912开光频率可以达到1MHz…
  • MAX14912配置为并行模式,但是在上电后无法正常输出,请问是什么原因?

    MAX14912通过外部引脚配置为并行模式,在器件上电时根据引脚配置来确定工作方式,但是在上电时,如果/CS引脚为低,内部逻辑被锁定,导致无法更新外部的设置,因此,为确保器件在上电后可靠工作,一定要保证在上电时CS引脚为高电平。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.