• Created
Was this helpful?
  • MAX14879在待机模式下是否可以接收数据?

    MAX14879在待机模式下,其接收器依然处于工作状态,也就是说,如果CAN接收器收到信号,则会反应在接收器输出端。但与正常工作模式相比,待机模式下的接收器具有不同的显性电平和隐性电平检测门限: 如果差分输入VDIFF > 1.15V,RXD输出逻辑低电平;如果VDIFF < 0.45V,RXD输出逻辑高电平。而正常工作模式下的检测门限分别为0.9V和0.5V。
  • 采用MAX1487作为主机,MAX485作为从机,总线上是否可以支持超过60个MAX485从机?

    总线上可以支持多少个从机设备是由从机的输入阻抗决定的,根据RS485规范,总线上可以带32个单位负载的从机设备,对于MAX485器件,该器件的输入阻抗为单位负载,因此无论选择何种器件作为主机,总线上只能带32个从机,如果选择MAX1487作为从机,因为MAX1487为1/4单位负载,因此总线上可以支持最多32*4=128个从机设备,如果需要支持超过60个从机,要选择MAX1487作为从机,主机可以选择MAX1487…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.