MAX14827AATG+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX14827A提供UART和SPI接口,是否可以同时使用?
SPI接口用于配置、监测IO-Link device的工作状况。 SPI工作时,外部UART可以连接到MAX14827A独立的UART接口引脚 (TX, RX, TXEN)工作,我们称这种模式为SPI/UART并行工作模式。拉低 UARTSEL引脚即可支持SPI、UART同时工作。
MAX14827A是否可以用在 IO-Link主机侧?
MAX14827A设计用于传感器侧,不能满足IO-Link主机的所有要求,比如,拉高C/Q发送唤醒信号。因此,与采用IO-Linke主机收发器相比,用MAX14827A连接两个传感器有些困难。但如果用户不要求满足IO-Link的所有要求,把MAX14827A用在主机侧也是可能的。
外部主站提供一个24V给从站的执行器使用,此时接口的2脚被占用,这种情况下MAX14827A的DI,DO引脚该如何处理?
根据IO-LINK标准,IO-LINK接口的pin2定义为悬空或者设置为DI或DO(port class A),也可以定义为P24(port class B),用于为器件提供额外电源。从您目前的描述来看,目前的主机将pin2定义为P24,在这种情况下,只能将MAX14827A的DI连接到pin2,或者将pin2悬空。MAX14827A的DO引脚不使用。 如果将DI连接到pin2, 可以用来检测P24是否上电…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.