• Created
Was this helpful?
  • 请问MAX14746芯片规格书中JEITA温度范围设定的意义是什么?

    为了提高锂电池充电的安全性,需要根据JEITA规范的要求,序言 降低低温和高温下的充电电流和电压。 具体到MAX14746,用户可以设置 电池温度位于0°C和10°C之间时,降低充电电流;电池温度为45°C和60°C之间时,降低充电电压;电池温度为0°C以下或者60°C以上时,停止充电。 可以参考下图的规范要求:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.