MAX13487EESA+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX1x
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX13487E在发送数据时会出现回声(接收器禁止),为什么?
MAX13487E这款RS485收发器具备自动收发控制功能,其接收器在关闭接收器(/RE = "1")时,接收器输出为高阻态(如下表),这一点与普通的RS485收发器有所不同。如果在RO引脚没有接上拉电阻,此时将会耦合噪声,产生所谓的“回声”。另外,为了建立可靠地通信,同样需要在RO引脚加上拉电阻。加上拉电阻后,确保Rx关闭时处于高电平,可解决这一问题。
MAX13487的输出电平不正确,什么原因?
MAX13487为自动方向控制RS485收发器,其发送器输出和接收器输出的高电平均为高阻输出,A/B线需要上、下拉电阻,接收器输出需要上拉电阻,以确保正确的输出电平。 工作在自动换向模式时。RE管脚需要拉高。
如何实现RS485的自动双向收发
标准的RS485芯片跟MCU之间应该有三根线,即数据发送DI/数据接收RO以及收发控制DE/RE,收发控制线高电平时为发送状态,低电平时为接收状态。对于需要数字和电源隔离的RS485通信环境,有些客户出于MCU资源紧张或降低成本,会考虑采用一种简化结构,即省去收发使能控制,而是把发送信号经过三极管反相后驱动收发使能控制。这种配置基本上也能实现RS485通信,但有些用户会反映通信稳定性不好,误码率高…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.