Post Go back to editing

MAXIMUM RESOLUTION SUPPORT IN SINGLE MIPI OUTPUT PORT OF AD-GMSL792MIPI-EVK

Category: Hardware
Product Number: AD-GMSL792MIPI-EVK

Hi,

I am using the AD-GMSL792MIPI-EVK kit, which has two MIPI output ports. I want to connect two 4K 60 fps YUV422 8-bit cameras to both inputs and take the output from a single MIPI output connector. Is this possible?

Please clarify the following queries:

  1. Can we connect two 4K 90 fps GMSL3 cameras and take the output through two separate MIPI output connectors?

  2. Can we take the output of one 4K 90 fps camera through a single MIPI output port?

  3. Is there any possibility of taking the output of two 4K 60 fps YUV422 8-bit cameras through a single MIPI port?

Regards,
Nitheesh

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.