Category: Datasheet/Specs
Product Number: MAX9295D
MAX9295手册中描述了芯片处于GMSL1模式下时具有GPO功能,但是我在实际将芯片置于GMSL1模式下时(将CFG_0、CFG_1的上下拉电阻设置为GMSL1 HIM Enabled COAX),在与对端GMSL1解串器(MAX9296运行在GMSL1模式和MAX96706都试过)连接后,对端传输过来的GPI信号(一个25HZ的frame sync信号)无法在对应的GPO引脚上测量到,对应的GPO引脚上始终保持相同电平;但是如果使MAX9295处于GMSL2模式下时可以正常接收到对端GMSL2解串器传输过来的GPIO信号;