你好!
我们现在使用max96716和max96717的GPIO透传功能,传输路径为:处理器产生fsync信号--》96716的MFP10--》GMSL2--》96717的MFP6--》sensor,目前的配置为:
//DES I2C Address=0x50
//SER I2C Address=0x84
//SER MFP6 Outputs FSYNC
0x84,0x02D0,0x84, // GPIO RX Tunnel Enabled, 1MΩ Pull-Down
0x84,0x02D1,0x66, // Pull-up, Push-pull, TX_ID=0x06
0x84,0x02D2,0x46, // RX_ID=0x06
//DES MFP10 Accepts FYSNC Signal
0x50,0x03E0,0x08, // FSYNC mode set to external
0x50,0x03EF,0x86, // FYSNC enabled on Pipe Y and Z
0x50,0x02CE,0x83, // GPIO TX tunnel enabled
0x50,0x02CF,0x66, // TX_ID=0x06
0x50,0x02D0,0x46, // RX_ID=0x06
但是现在96717的MFP6量不到正确的信号,请问是什么原因呢?
谢谢