Post Go back to editing

max96717f的csi接口能否兼容csi-2 v2.0

Thread Summary

用户询问MAX96717F的CSI-2 V1.3接口是否能兼容传感器的CSI-2 V2.0输出,特别是ECC校验位长度不同。建议检查传感器是否可以配置为输出兼容低版本MIPI接收器的数据。
AI Generated Content

我这边用的传感器输出的CSI接口是CSI-2 V2.0的,max96717f的数据手册中说明其CSI接口上 CSI-2 V1.3的

参考mipi的标准,这两个版本的数据中ecc校验位的长度不同,不清楚max96717f的csi接口能否兼容CSI-2 V2.0版本,需要对那些寄存器进行设置。