Hello,
I am a thermal engineer and I am interested in implementing MAX96716AGTM/VY+T GMSL in my PCB.
I went through the component's datasheet and could not find the following information:
1. Exposed pad dimensions (or even better, a mechanical drawing of the component).
2. Thermal resistance from junction to board.
3. It is also mentioned that the thermal resistance junction to case is 1°C/W. Is it the case top or bottom? If it is the case top then I am missing the case bottom resistance, and vise versa.
4. It is unclear what is the maximum junction temperature, is it -40°C to 105°C?
Thank you in advance,
Adi