There are design files for MAX96717/F/R EVKit, and this is just great. But is there binary file for MK20DX256VLH7 which is the core of the EVK?
I want to build the kit myself, and this is the only thing missing.
There are design files for MAX96717/F/R EVKit, and this is just great. But is there binary file for MK20DX256VLH7 which is the core of the EVK?
I want to build the kit myself, and this is the only thing missing.
There's prebuilt image of teenzy core, installed with GUI. However, the source code of this image will not be made public.
oh, I dont need a source code. So I can just put the black uC onto the board and flash it with GUI?
Can you elaborate on this? Because tech support keeps responding me with nonsense
EU team should be supporting you for detailed questions.
Here, I personally, think your plan is correct. You need to be careful of the hardware design, especially in PINOUT and address assignment. Everything needs to be exactly same with EVK. Then the firmware can work normally.
tech support keep sending link to their linux github repository, and this worries me, because I dont want to spend couple of hundreds euros on pcb and components just to end up with dead board