Post Go back to editing

Configuration for MAX9277 & MAX9276

Thread Summary

The user asked if the MAX9277 serializer can interface with the MAX9276 deserializer. The final answer confirmed that it is possible and recommended referring to the evaluation kit user guides for both chips for necessary settings and configurations.
AI Generated Content
Category: Hardware
Product Number: MAX9277

Hello,

Can I interface MAX9277 serializer with MAX9276 deserializer.

Whether it will work, if works what are all the changes or settings to be updated.