Post Go back to editing

Can the main i2c port also function as pass through i2c ports?

Category: Hardware
Product Number: MAX96717

I am looking at the max96717/MAX96716. I will need both i2c and SPI port relay functions across the gmsl link. It looks like the I2C pass through pins share the SPI pins. I wanted to know if the main i2c port also functioned as a pass through port? 

My i2c master (uC) is on the max96716 side, is it assumed that the i2c main ports on the remote device is connected to the pass through pins?

Parents Reply Children
No Data