Post Go back to editing

max96724聚合问题

Thread Summary

The user inquires if a 4LINE D-PHY can handle the aggregated output from three cameras (2*8MP + 3MP) running at 30FPS. The final answer calculates the total pixel clock and bandwidth, concluding that the required 10944Mbps exceeds the 10Gbps D-PHY limit. An accompanying answer suggests considering video pipeline mode 1 with 12bpp to reduce bandwidth, but the default mode 2 is more commonly used.
AI Generated Content
Category: Hardware
Product Number: MAX96724R

96724 GMSL3个输入,分别是2*8MP+3MP,都是30FPS的摄像头,后端聚合输出用1个4LINE的D-PHY,是否可以?