Post Go back to editing

GMSL GUI工具使用

Thread Summary

The user inquires about connecting a custom board to the GMSL GUI for debugging. The final answer states that the GMSL GUI can only connect to official ADI evaluation boards, and custom hardware requires a similar design to the evaluation board. The user can use the evaluation board to generate configuration scripts, which can then be implemented by their embedded developers. The GUI and related documentation can be downloaded from the product homepage of public devices like MAX96717/MAX96724.
AI Generated Content

ADI工程师,您好

当前已下载好贵司的GUI工具,如下图

想通过上位机调试我司的样机

样机如何与上位机相连,需要I2C转USB工具吗?

还是ADI有专门的工具?

有关于这个GUI的使用说明吗?

Parents Reply Children
No Data