Hi Sir,
Could you help to check , Is the MAX9257A compatible with MAX9288A?
any reference setting or design considerations?
BR
Justin
Hi Sir,
Could you help to check , Is the MAX9257A compatible with MAX9288A?
any reference setting or design considerations?
BR
Justin
Any suggestions ?
BTW , is MAX9257A comptible with MAX9278A?
MAX9257A is not a GMSL SerDes product. It is not compatible with GMSL products.
Hi Mason,
thansk for your support , another question , is MAX9257A and MAX9258A can support BT656 transmission?
MAX9257/MAX9258 use VSYNC signal to enter/exit the control channel phase, whereas BT656 does not have sync signals. Without VSYNC, control channel cannot be used.
Hi Mason,
if our SOC can output BT656+Hsync and Vsync , MAX9257A and MAX9258A will working well?
Thanks for your support.
I think it's OK. But you need to take care of the VSYNC timing requirements according to the datasheet.