MAX17263外部所接LED用于指示电池电量,其点亮数量与电量的关系会受LEDCfg1 (040h)的GrEn位影响。
1. 假设MAX17263外部接了6个LED,当GrEn=1时,使用100%除以6,得到16.7%;如果电量等于0时,没有LED点亮,电量在0%到16.7%之间时1个LED点亮,以此类推,当电量高于83.3%时6个LED全部点亮;
2. 假设MAX17263外部接了6个LED,当GrEn=0时,使用100%除以6,得到16.7%,16.7%再除以2得到8.33%;如果电量低于8.33%时,没有LED点亮,电量在8.33%到25%之间时1个LED点亮,电量在25%到41.67%之间时2个LED点亮,以此类推,当电量高于91.67%时6个LED全部点亮。