文档 将nLearncfg 寄存器设置为 0x2672 后MAX17205G充电电量不准,什么原因?
  • 问答
  • 文档
  • 成员
  • 标签
  • Cancel
  • 文档
  • +AD9161: FAQ
  • +DS2438: FAQ
  • +DS2704G+: FAQ
  • +DS2711E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • +DS2740: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762: FAQ
  • +DS2764: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • DS2780: FAQ
  • +DS2780E+: FAQ
  • +DS2781AE+/: FAQ
  • +DS2781E+: FAQ
  • +DS2781G-A2+: FAQ
  • +DS2782E+: FAQ
  • +DS2784 EEPROM PROG: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • +DS2788E+: FAQ
  • +MAX14690AEWX+: FAQ
  • MAX14745: FAQ
  • MAX14745AEWX+: FAQ
  • +MAX14745AEWX+T: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+T: FAQ
  • +MAX17043: FAQ
  • +MAX17047G+: FAQ
  • +MAX17048: FAQ
  • +MAX17049G+: FAQ
  • +MAX17055AEWL+: FAQ
  • +MAX17058: FAQ
  • +MAX17201/MAX17205: FAQ
  • +MAX17201G+T: FAQ
  • MAX17205: FAQ
  • -MAX17205G+: FAQ
    • 4节串联的锂电池接到MAX17205评估板后,评估板软件显示有错误,原因是什么?
    • MAX17201/17205的I2C从机地址是什么?
    • max17205 在测量电流为负时,如何根据测量的数字信号来计算电流值。比如Current值为0xF163 即 61795,怎么算出来是-584.531?
    • MAX17205内部的过流比较器带有一个可编程的去抖延迟设置,请问该比较器具体是如何工作的?
    • MAX17205在设置电池容量是直接将数据转换成16进制数据写入nDesignCap Register(1B3h)吗?
    • MAX17205如何检测电池的温度,要配置哪些寄存器,读哪些寄存器?
    • MAX17205应该设置哪些寄存器才能读到正确的剩余电量?
    • MAX17205是否支持镍隔、镍氢电池等?
    • max17205的i2c访问地址应该是0001011x还是0010110x ?
    • 使用MAX17205时,软件读出的电压、电流、温度数据都正确,但RepSOC始终为1.0%,为什么?
    • 在使用MAX17205时读取的温度值不正确,因此,想通过读取nPackCfg寄存器来验证I2C通讯的正确性,期望读取到默认的0xa02,而实际得到的是0x05,可能是没有正确理解内部寄存器的地址是如何映射的,能详细介绍一下这方面的内容吗?
    • 在使用MAX17205测量电量时,读取电池电压和器件名称正确,但是读取的电流值始终为0,请问是什么原因?
    • 如何使用MAX17205获取电池电量?
    • 将nLearncfg 寄存器设置为 0x2672 后MAX17205G充电电量不准,什么原因?
    • 读取MAX17205的哪个寄存器,来获取电池是充电还是放电状态。
    • 针对大容量、多节串联的锂离子电池,有没有比较好的电量计方案?
  • +MAX17205G+T: FAQ
  • +MAX17211G+: FAQ
  • MAX17260: FAQ
  • +MAX17260BEWL+: FAQ
  • +MAX17261METD+: FAQ
  • +MAX17261XEVKIT: FAQ
  • +MAX17262 EVALUATIO: FAQ
  • +MAX17262MEWL+: FAQ
  • +MAX17263: FAQ
  • +MAX1737: FAQ
  • MAX17435ETG+: FAQ
  • +MAX17435ETG+T: FAQ
  • +MAX17435EVKIT+: FAQ
  • MAX17572: FAQ
  • +MAX17572ATC+: FAQ
  • +MAX17830GUN/V+_T1: FAQ
  • MAX17841BGUE/V+: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20303 EV KIT SOFTWARE: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20335AEWX+T: FAQ
  • +MAX6951CEE+: FAQ
  • +MAX6955AAX+: FAQ
  • +MAX6956: FAQ
  • +MAX6958AAEE+T: FAQ
  • MAX7032: FAQ
  • +MAX7032ATJ+: FAQ
  • +MAX7034AUI+: FAQ
  • MAX77650A: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+T: FAQ
  • MAX77651AEWV+: FAQ
  • +MAX77651AEWV+T: FAQ
  • +MAX77654AENV+: FAQ
  • MAX77734: FAQ
  • MAX77734AENP+: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77818EVKIT: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+_P1: FAQ
  • +MAX8713ETG+: FAQ
  • +MAX8971: FAQ
  • 能源存储系统(ESS)和电池管理系统(BMS) 标签

将nLearncfg 寄存器设置为 0x2672 后MAX17205G充电电量不准,什么原因?

 

MAX17205的nLearncfg 寄存器如果使用默认的0x2602,则前两个充放电周期会以OCV为准估算电量,这样即使第一次上电时MAX17205估算的电量误差较大,充满电后得到的电池总电量也不会过大,而且经过两个完整的充放电周期后nLearncfg 寄存器会自动更新为0x2672,MAX17205将以库仑计为主来估算电量。而如果在第一次接电池时就将nLearncfg 寄存器设置为 0x2672,则在第一充电时MAX17205会以库仑计的方式估算电量,这会造成其计算出来的电池总电量远大于或小于电池真实总电量。

Tags: KA-01419 MAX17205G+ MAX17205,nLearncfg 寄存器
  • Share
  • History
  • Cancel
 
Related Content
  • What is the MAX17205 I2C address?
    MSDAPI
    The two I2C slave addresses for the MAX17205 are 0x6C and 0x16 as shown in Table 27 of the datasheet. Each address is used to access a separate portion of the internal memory.
  • MAX17205G+: FAQ
    MSDAPI
    MAX17205G+: FAQ
  • MAX17205G+: FAQ
    MSDAPI
    MAX17205G+: FAQ
 
Related Content
  • What is the MAX17205 I2C address?
    MSDAPI
    The two I2C slave addresses for the MAX17205 are 0x6C and 0x16 as shown in Table 27 of the datasheet. Each address is used to access a separate portion of the internal memory.
  • MAX17205G+: FAQ
    MSDAPI
    MAX17205G+: FAQ
  • MAX17205G+: FAQ
    MSDAPI
    MAX17205G+: FAQ