文档 AD9164 phase noise plot in data sheet has a bump at around 10 kHz offset. What causes it?
  • 问答
  • 文档
  • 成员
  • 标签
  • Cancel
  • 文档
  • -AD9161: FAQ
    • AD9164 phase noise plot in data sheet has a bump at around 10 kHz offset. What causes it?
  • +DS2438: FAQ
  • +DS2704G+: FAQ
  • +DS2711E+: FAQ
  • +DS2712EVKIT+: FAQ
  • DS2715: FAQ
  • +DS2715BZ+: FAQ
  • +DS2740: FAQ
  • +DS2745EVKIT+: FAQ
  • +DS2745U+: FAQ
  • +DS2762: FAQ
  • +DS2764: FAQ
  • +DS2775G+: FAQ
  • +DS2777: FAQ
  • DS2780: FAQ
  • +DS2780E+: FAQ
  • +DS2781AE+/: FAQ
  • +DS2781E+: FAQ
  • +DS2781G-A2+: FAQ
  • +DS2782E+: FAQ
  • +DS2784 EEPROM PROG: FAQ
  • +DS2784G+: FAQ
  • +DS2786: FAQ
  • +DS2788E+: FAQ
  • +MAX14690AEWX+: FAQ
  • MAX14745: FAQ
  • MAX14745AEWX+: FAQ
  • +MAX14745AEWX+T: FAQ
  • MAX14921: FAQ
  • +MAX14921ECS+T: FAQ
  • +MAX17043: FAQ
  • +MAX17047G+: FAQ
  • +MAX17048: FAQ
  • +MAX17049G+: FAQ
  • +MAX17055AEWL+: FAQ
  • +MAX17058: FAQ
  • +MAX17201/MAX17205: FAQ
  • +MAX17201G+T: FAQ
  • MAX17205: FAQ
  • +MAX17205G+: FAQ
  • +MAX17205G+T: FAQ
  • +MAX17211G+: FAQ
  • MAX17260: FAQ
  • +MAX17260BEWL+: FAQ
  • +MAX17261METD+: FAQ
  • +MAX17261XEVKIT: FAQ
  • +MAX17262 EVALUATIO: FAQ
  • +MAX17262MEWL+: FAQ
  • +MAX17263: FAQ
  • +MAX1737: FAQ
  • MAX17435ETG+: FAQ
  • +MAX17435ETG+T: FAQ
  • +MAX17435EVKIT+: FAQ
  • MAX17572: FAQ
  • +MAX17572ATC+: FAQ
  • +MAX17830GUN/V+_T1: FAQ
  • MAX17841BGUE/V+: FAQ
  • +MAX17841BGUE/V+T: FAQ
  • MAX17843ACB/V+: FAQ
  • +MAX17843ACB/V+_T1: FAQ
  • +MAX1873TEEE+: FAQ
  • +MAX20303 EV KIT SOFTWARE: FAQ
  • MAX20303AEWN+: FAQ
  • +MAX20303AEWN+T: FAQ
  • +MAX20335AEWX+T: FAQ
  • +MAX6951CEE+: FAQ
  • +MAX6955AAX+: FAQ
  • +MAX6956: FAQ
  • +MAX6958AAEE+T: FAQ
  • MAX7032: FAQ
  • +MAX7032ATJ+: FAQ
  • +MAX7034AUI+: FAQ
  • MAX77650A: FAQ
  • +MAX77650AEWV+: FAQ
  • +MAX77650BEWV+T: FAQ
  • MAX77651AEWV+: FAQ
  • +MAX77651AEWV+T: FAQ
  • +MAX77654AENV+: FAQ
  • MAX77734: FAQ
  • MAX77734AENP+: FAQ
  • +MAX77734AENP+T: FAQ
  • +MAX77818EVKIT: FAQ
  • MAX77818EWZ+: FAQ
  • +MAX77818EWZ+_P1: FAQ
  • +MAX8713ETG+: FAQ
  • +MAX8971: FAQ
  • 能源存储系统(ESS)和电池管理系统(BMS) 标签

AD9164 phase noise plot in data sheet has a bump at around 10 kHz offset. What causes it?

Question:

There is a "bump" in the phase noise plots in the AD9164 data sheet (Figure 38 and 41). It looks like some filter(s) that kicks in at these frequencies. What is causing these bumps/increase of phasenoise ? Can this be improved/attenuated ?

Resolution:

That bump is from regulator power supply noise and the phase noise from the signal generator used for the DAC clock input during characterization. For information on improved phase noise performance and contributors to phase noise, please check this article in Analog Dialogue. http://www.analog.com/en/analog-dialogue/articles/analyzing-and-managing-the-impact-of-supply-noise-and-clock-jitter-on-high-speed-dac-phase-noise.html

Tags: ad9161 high-speed dacs KA-01046 phase noise ad9164